Project No. 1: UVNA-63
DIY Vector Network Analyzer

Instructions for Assembly

- An 8 lb-in calibrated torque wrench is recommended for interconnection of components in this kit.
- Keep connectors clean from foreign objects and debris to ensure accurate measurements.
- When making SMA connections, always hold the female connector steady using the anti-torque nut while rotating the male SMA connector coupling nut to avoid cross-threading or damage to the connectors.


BILL OF MATERIALS
Kit Components:





Browse all RF attenuators