This power meter, based on a Mini-Circuits ZX47 power detector, gives a direct display of -55 to +10 dBm power levels.

The modularized spectrum analyzer, as described by Scotty Sprowls (www.scottyspectrum analyzer.com), cannot align in the low GHz range. The frequency meter will go up to 3.5 GHz and give a reading, but no indication of the power level involved. Hence, a 100 MHz scope cannot cope and will be useless. Two types of measurements are needed:

  • Relative measurements: Is there any loss or gain? How much? Is the signal getting from point A to B?
  • Absolute measurements: Is the required 10 dBm coming from the phase locked oscillators (PLO’s)? When making absolute measurements a sine wave shape is assumed. In addition, all of the power coming out of the device must be measured; placing the probe in parallel when the device is delivering power to another device, will not measure the true output. Most likely, assuming 50Ω impedances, it will measure 50% of the power. Use a pigtail attached to the meter as shown in Figure 1.
Figure 1: The finished assembled power meter.

The Problem

With tiny surface mount components diverting attention from the circuit, glancing at a meter on another device may result with the measuring probe slipping away with disastrous effects. When measuring voltages, it is possible to bring the handheld DVM very close to the point of measurement to see the results, but not the heavyweight HP 435B power meter. There needs to be a handheld device with local readout. This is particularly important in today’s crammed circuits where it is difficult to look away from the point of measurement, lest the probe start to slip.

The solution

As an alternative, the Mini-Circuits ZX47 power detectors measure RF power from 10 MHz to 8 GHz. Depending on the detector chosen, -50 dBm to +15 dBm, it will also display the results directly in dBm. This is especially convenient because with its small size, the readout can be at the place of measurement.

These devices are very linear, tiny, and have a wonderful dynamic range. Their data sheets include response curves that allow for a close calibration without the need for an external reference. Figure 3 shows the output voltage vs. input power response curves for the ZX47-40-S+ power detector. The device’s response runs true to the published curves between 1 and 2 dBm.

The combination of a VFO at 1013.3 MHz and this meter will allow the user to set up the spectrum analyzer’s cavity band-pass filter to a loss of -10 dB in no time flat.

Mini-Circuits offers four detectors in its ZX47 series. The linear span is approximately as follows :

  • Model 60: -55 to + 0 dBm.
  • Model 55: -50 to +5 dBm.
  • Model 50: -45 to +10 dBm.
  • Model 40: -40 to +15 dBm.

These ranges are good up to 6 GHz, but beyond that the range is smaller. Their output voltage is 0.6 to 2V. Since its high-power range may be increased by using an attenuator, my favorite is model 60.

The schematic shown in Figure 4 is quite simple: one potentiometer sets the slope and the other sets the intercept of the response curves. Since, up to 6 GHz, the linear portions are essentially parallel, the slope pot is set once and left alone. As Figure 3 shows, the 8 GHz output voltage curve is quite noticeably different than the lower frequency curves, and would require a different calibration. The intercept is a function of the frequency and is set at the time of calibration or simply taken from the Mini-Circuits curves.

Figure 2: A Mini-Circuits ZX47-40+ power detector module.
Figure 3: This graph shows the ZX47-40-S+ power detector output voltage vs. input power at 25°C. This graph is reproduced from the Mini-Circuits data sheet for the detector.
The schematic diagram of the power meter shows how simple this circuit is. Potentiometer R7 sets the detector slope for the LCD voltmeter and R8 sets the display intercept. Once the slope is set no further adjustments are needed to that control. The intercept potentiometer is adjusted for the appropriate frequency range.

The user interface includes a Lascar EMV 1125 LCD digital voltmeter, a bicolor LED (red when the switch is in calibration mode, green when in measurement mode) and the offset potentiometer. A calibration table is pasted to the face of the box (not seen in any of the pictures). The offset potentiometer is set to the value in the table, which corresponds to the frequency of the signal being measured.

The meter requires an external supply from 12 to 20V DC. Because of the detector current draw (about 120 mA), no attempt has been made to use batteries.

Figure 5 depicts the original unit. The left side of part A has the 12V jack. There was a 7805-voltage regulator bolted to the box floor underneath the circuit board. Both the regulator and the circuit board were secured by the screw visible at the top left corner of the circuit board. The IC visible on the circuit board is a charge pump to get the -5V needed for the Lascar LCD voltmeter. It is possible to build another version and move all the components to the printed circuit board that has simplified wiring. Figure 6 is a picture of the inside of the other version.

Figure 5: The original unit. The left wall in Part A has the 12V jack. There is a 7805 voltage regulator bolted to the box floor underneath the circuit board and secured by the screw at the upper left corner which holds both the 7805 and the circuit board in place. The IC visible on the circuit board is a charge pump device to get the -5V needed for the LASCAR LCD voltmeter. The latest version of the meter has moved all the components to the circuit board, which has simplified the wiring. Part B shows the front of the box, with the LCD voltmeter, the Calibrate/Measure switch, the intercept potentiometer control and the bi-color LED.

Construction Notes

It is possible to use a Hammond 1590A cast aluminum enclosure, and remove some material from the corners to make room for the Mini-Circuits detector as shown in Figure 7. Center punch the area and then use a drill, taking care not to engage it and go through the wall. The probe SMA hole offset is to provide clearance for the LCD in the other side of the box. The hole drilled on the box “floor” to secure one of the legs of the detector is not shown.

Some versions of the 7662-charge pump require that the LV pin (pin 6) be tied to the ground in order to ensure a -5V output of the same level as the positive input (Figure 6). Version 1.3 of the circuit board, which is the one shown in Figure 6, requires installing a wire jumper to ground. Circuit board version 1.4 has provision for a 0Ω resistor (R6) if needed.

Figure 8 shows the Lascar LCD voltmeter control board on the inside of the Hammond project case with the circuit board and power detector ready to be installed. Notice that the wires from the display, feed through a hollow stud on the back of the display, and they attach to a row of holes along the top of the control board as well as to the switch and R8 on the circuit board.

Figure 9 shows the bottom of the circuit board, with a 90° angled SMA male to female connector between the detector output and main circuit board. Use a ¼-inch length of 141 coax between the SMA female end and the circuit board. Do not solder the coax to the SMA connector until it is certain that everything fits correctly.

Figure 10 is the circuit board artwork. Note that this is a double-sided circuit board, with the traces on top of the board outlined in black and traces on the bottom of the board shown in lighter gray.

The circuit board file was created using ExpressPcb. Because ExpresPcb requires a minimum board size of 3.8 x 2.5 inches, builders may want to join with a few others to make the price more attractive. Another option would be to include boards for other projects with the order. Yet another alternative is to redo the design using Eagle.

A color copy of this artwork, along with the ExpressPCB file is available for download from the ARRL QEX files website: http://www.arrl.org/qexfiles. Look for the file 7x11_Hontoria.zip.

Drilling the Enclosure Cover:

The potentiometer requires a 5/16-inch hole, the LED requires 3/16-inch hole,  and the switch needs a 1/4-inch hole for the shaft. Refer your measurements to the centers of the enclosure screw holes, not to its walls. Then, transfer those measurements to the cover.

Setting Up the LASCAR LCD Voltmeter: 

The EMV1125 doesn’t require a split rail power supply. It can run from a single rail. Under these conditions, however, the signal must be left floating (totally isolated) from the power supply and link L2 ties with the floating signal (INLO) to a reference voltage (Com, held 2.8V below V+). Since in the power meter the signal is not floating, link L2 must be cut. Leaving this link will short GND to V+, damaging the meter. Figure 11 shows the LCD voltmeter control board, with the connections to the display.

The meter is thus operated from a ±5V split-rail supply. In order for the LCD to read 2V full scale the Ra (910 kΩ) and Rb (100 kΩ) resistors must be installed and link La must be cut. To set the decimal point so that the meter reads directly in dBm, the decimal link DP1 must be shorted out.

Finally, measure the input voltage at IN-HI with an accurate DMM, and adjust CAL for the same reading on the Lascar display.

Figure 6: A look inside the newest version of the meter. The trimmer is the slope setting and the miniature potentiometer is for the intercept setting. Note the glob of glue on the right securing the board to the detector.
Figure 7: Using a Hammond 1590A cast aluminum enclosure to remove some material from the corners to make room for the Mini-Circuits sensor. Center punched the area and then used a drill, taking care not to engage it and go through the wall. The probe SMA hole offset is to provide clearance for the LCD in the other side of the box. Not shown here, there was a hole drilled on the box “floor” to secure one of the sensor legs.
Figure 8: The LCD voltmeter comes with fairly long wires, which was used to connect it to the circuit board.
Figure 9: Insert a 1/4-inch length of 141 coax into right angled SMA connector to provide clearance between the detector and the circuit board. The coax (shield and center conductor) should not be soldered to the SMA until the very end.
Figure 10: This control board is part of the Lascar voltmeter. The wires from the display connect to the top row of holes.
Figure 11: This is the circuit board artwork. The board is 2.4 x 1-inch.
Table 1

Preliminary Calibration

The preliminary calibration uses the Mini-Circuits data sheet curves. A more precise calibration will require comparison with another power meter. The following is how the preliminary calibration is performed.

If using the Lascar EMV1125, set it up in accordance with its data-sheet and the instructions above. If using any other meter, set it up to display 2V, but move the decimal point to one decimal digit.

Refer to the schematic diagram in Figure 4. It refers to the designation of the potentiometers. This preliminary calibration procedure is based on setting the slope with R7 and the intercept with R8.

  1. Set the switch to “Calibrate” position, to ground the EMV 1125 input line; the bi-color LED should turn to red. Do not connect any signal to the RF input of the ZX47. Turn on the power supply.
  2. Use a DMM to measure the voltage at the ZX47 output (the top of resistor R1). Suppose you measure 2.17V.
  3. Adjust the slider of the slope potentiometer R7 (the small trimmer on the circuit board) and measure the voltage at the arm. For this example you should measure 2.17V x 0.4 = 0.868V.
  4. Use the Model 40 Mini-Circuits detector with the curves shown in Figure 3, reproduced from Mini-Circuits data sheet. Use a signal generator to inject a 10 MHz signal to the ZX47 -40+ RF input. Ideally, the signal level should be in the center of the range, which for the Model 40 is around -15 dBm. In any case, do not exceed the upper limit for the ZX47 detector you are using. Read the voltage at the input side of R1. Suppose it read 1.38V.
  5. Look at the Figure 4 graph. The thin black line corresponds to 10 MHz and 1.38V corresponds to -14 dBm.
  6. Set the switch to the “Measure” position; the bi-color LED will be green. Adjust the intercept potentiometer (R8) until you get the same dBm reading on the Lascar display. Return the switch to “Calibrate” and make a note of the reading on the display. That is your set point at 10 MHz
  7. Set the switch to “Measure” again, and you are ready to start measuring power in the 10 MHz range. You can now experiment with different frequencies and levels. For example, a set point at 50 MHz is 44.7, and a set point at 1000 MHz it is 43.8. These set points are the equivalent of calibration factors used in other instruments. Table 1 shows the calibration table for the meter.

Background

With Model 40, the response equation at 10 MHz is: dBm (10 MHz) = 42 – (40 x V) For example, a sensor voltage output of 1.3V corresponds to a power input of 42 – (40 x 1.3) = 42 – (52) = -10 dBm at 10 MHz (the thin black line on Figure 3). For other frequencies, the response equations are: dBm (1000 MHz) = 41.7 – (40 x V) dBm (2000 MHz) = 39.25 – (40 x V) dBm (6000 MHz) = 44.7 – (40 x V) dBm (8000 MHz) = 52 – (40 x V)

Since the lines are essentially parallel (with the exception of the 8 GHz line) the slope has been set as a constant at 40. The intercepts are frequency dependent, however. Based on the Mini-Circuits graphs, the Model 40 power detector should provide fairly close results to the above formulae between -35 and +15 dBm.

Browse all RF power detectors

%d bloggers like this: