Engineering Resources
Filter By Category:

Synthesizer Design
The design example covered here is an 800 to 900 MHz synthesizer in 100 kHz steps with a minimum output power of 10 mW across the band. Mini-Circuits model POS-1060, a low noise voltage controlled oscillator that operates over the range of 750 to 1060 MHz, is used.

Reducing Power Supply Noise in VCOs
It is always a good design philosophy to provide RF bypassing of power and DC control lines to the VCO. This is indeed the case when the VCO is located some distance away from the power supply.

Constant-Impedance IF Band-pass Filters Improve Circuits Performance
Double-balanced mixers are normally very wideband. When used as down converters, the sum and difference of frequencies are of equal amplitude. Filtering is essential to remove the sum frequency.

Methodology for Computation of Maximum Power Handling in LTCC Low-Pass Filters
LFCW series filters are made using LTCC (low temperature co-fired ceramic) technology. Due to low losses and high temperature handling capability of the ceramic material, they can handle reasonably high power levels, even though they are of small size.

VCO Test Methods
Well regulated power supplies are recommended for tuning and VCO supplies. Bias tee's in the DC and tuning voltage lines help reduce the power supply noise. This article will cover information on tuning, harmonics and spurious level and more.

An Introduction to Filters
In the operation of electronic systems and circuits, the basic function of a filter is to selectively pass, by frequency, desired signals and to suppress undesired signals. The amount of insertion loss and phase shift encountered by a signal passing through the filter is a function of the filter design.

An Introduction to Frequency Multipliers
Mini-Circuits' frequency multipliers offer a new degree of freedom in designing frequency multiplier chains. Their multi-octave band width and excellent rejection of fundamental and third harmonics enable a significant reduction in filter requirements.

DAT-31R5A/31A/15R5A Series Evaluation Boards Operation to VDD=5.2V
Mini-Circuits DAT series of 50Ω digital step attenuators support a wide variety of configurations including attenuation range, step size and operating power supply voltages. Read further for more information.

Band-pass Filters with Linear Phase Response
Filters with linear phase response are desirable, due to their flat group delay, in many applications, for example in image processing and digital data transmission. Such filters maximally preserve the wave shape of the passing signal, since they delay all frequency components of the signal by the same amount.

DIY Low-Cost Power Splitters
There is a continuing demand to reduce the cost and increase the performance and quality at the same time. Mini-Circuits is working to satisfy these goals and has introduced a new splitter series to meet the demands of the market.

Super Wide-band RF Choke
Use of heterojunction bipolar transistor technology has resulted in development of super wide-band monolithic microwave amplifiers such as Mini-Circuits ERA series. These amplifiers cover a bandwidth from DC to 8 GHz.

High Power Limiter Modules
In many applications, front end filtering is used to protect the receiver from unwanted high-power signals, but even with this reinforcement, high-power signals may still be present. A limiter can be used in a broadband device that will not degrade receiver sensitivity.