RF coaxial cable image shown in longitudinal view with the conductive and dielectric layers cut away and exposed.

Signal integrity is critical in every RF and microwave system. Whether you are designing a complex satellite communications array, setting up a 5G test environment, or running precision measurements in a lab, the performance of your interconnects will play an important role in overall system performance. Among these interconnects, the RF Cable is often underestimated. Engineers tend to focus on components such as amplifiers, filters, and antennas – and rightfully so – but the wrong cable choice can quietly compromise results, introduce unnecessary losses, and even cause system failure.

At Mini-Circuits, we have spent decades leading the engineering of RF cables that meet the most demanding requirements across industries like aerospace, defense, telecommunications, and test and measurement. Our catalog includes a wide range of radio frequency cable products, including:

  • Ultra-flexible HandFlex® assemblies to rugged armored cables for high-frequency vector network analyzer (VNA) measurements.
  • Various RF cable connector types to suit every application, including SMA, N-type, 2.92mm, BNC, and custom configurations.

This guide gives engineers, technicians, and procurement professionals an in-depth look at RF cables, including:

  • What they are
  • The nuances of how different RF cable types work
  • Differences between various types
  • How to select the best RF cable for your project

We will also explore RF cable connector types, attenuation and loss calculations. By the end, you will better understand the process of choosing the best RF cable for your specific application, with confidence that your choice will deliver optimal electrical performance, mechanical durability, and cost-effectiveness.

The Mini-Circuits Difference

Mini-Circuits’ approach is rooted in both engineering precision and practical application. For example, our phase-stable cables are designed to maintain electrical length under flexure, ensuring repeatable measurements in dynamic test setups. Our low-loss cables deliver minimal attenuation over long runs, making them ideal for base station feeder lines and distributed antenna systems. Our RF cable connector catalog is mechanically robust, providing secure, repeatable connections that protect against environmental stress and frequency-related degradation.

Choosing the right RF cable centers on integrating a reliable signal pathway into your system architecture. The wrong choice can lead to mismatched impedance, increased return loss, or environmental failure. The right choice reinforces consistent performance, reduced maintenance, and better overall ROI.

Click the links below to jump to any chapter in this guide.

  • What defines a radio frequency cable?
  • The role of coaxial cables in RF systems
  • Key types of RF cable assemblies
  • Detailed breakdown of RF cable types and their applications
  • Standard and custom RF cable connector types
  • How to choose the right size and configuration

What is an RF Cable?

An RF cable, also referred to as a radio frequency cable, is a specialized transmission line designed to carry high-frequency electrical signals with minimal loss and distortion. Unlike general-purpose wiring, an RF Cable is engineered to maintain consistent impedance, reduce signal reflection, and protect against electromagnetic interference (EMI) and radio frequency interference (RFI).

The most common RF cables are coaxial in design, meaning they have a central conductor, dielectric insulation, an outer conductor (shield), and a protective jacket. This geometry ensures the signal is carried in a controlled electromagnetic environment, with the outer shield preventing signal leakage and protecting against external noise.

Key design parameters include:

  • Characteristic Impedance: Usually 50 ohms for most RF applications or 75 ohms for video and certain broadband systems.
  • Frequency Range: Determines how high in frequency the cable can perform effectively without excessive loss or phase instability.
  • Attenuation: Measured in dB per unit length, this indicates how much signal power is lost over distance.
  • Shielding Effectiveness: The ability to reject unwanted interference.

Typical applications of radio frequency cables include:

  • Wireless infrastructure (base stations, DAS systems)
  • Aerospace and defense communications
  • Medical imaging and diagnostic equipment
  • Test and measurement setups (VNAs, spectrum analyzers)
  • Broadcast and video production
  • Industrial IoT sensor networks

At Mini-Circuits, we design our flagship RF cables with application-specific performance in mind. Our HandFlex® series offers ultra-flexibility for compact routing, while our armored VNA cables ensure mechanical durability for field and lab use at frequencies up to 110 GHz.

Coaxial Cable: What is it Used For?

The coaxial cable is the most common RF cable type. Its name comes from the fact that the central conductor and outer conductor share the same geometric axis. This precise structure controls impedance and minimizes radiation losses.

What is the structure and components of an RF cable?

  • Inner Conductor: Carries the RF signal.
  • Dielectric: Maintains spacing between conductors, controls velocity factor.
  • Shield: Braided, foil, or both — prevents signal leakage and blocks EMI/RFI.
  • Outer Jacket: Provides environmental and mechanical protection.

What are the primary uses of an RF cable?

  • Signal Transmission in RF Systems: From antennas to radios, a coaxial radio frequency cable maintains low loss and minimal reflection.
  • Test and Measurement: Lab-grade coaxial cables ensure accurate, repeatable measurements.
  • Broadcasting: Coax runs and transmits high-quality video and audio signals.
  • Military/Aerospace: Armored and high-shielding coax cables withstand extreme vibration, temperature, and pressure.

Mini-Circuits’ coax RF cables cover frequencies from DC to 110 GHz, supporting applications in radar, satellite, wireless infrastructure, and 5G test environments.

What are the advantages of RF cables?

  • Controlled impedance (typically 50 or 75 ohms)
  • High shielding effectiveness
  • Wide bandwidth capability
  • Ease of termination with standard RF cable connector types

In short, coaxial cables are the workhorses of RF signal transmission, and selecting the right one is essential for optimal performance.

RF Cable Assemblies

An RF cable assembly is a complete interconnect solution — cable plus connectors — built and tested to deliver guaranteed electrical performance. Each Mini-Circuits RF cable comes equipped with:

  • Pre-terminated with precise RF cable connector types
  • Factory-tested for VSWR, insertion loss, and phase stability
  • Easy installation time, reducing human error

Mini-Circuits offers:

  • HandFlex® Assemblies: Ultra-flexible, small bend radius, ideal for confined spaces
  • Precision VNA Cables: Phase stable to 110 GHz for high-accuracy measurements
  • Armored Cables: Added durability for field and industrial environments

Assemblies also ensure compatibility between cable type, connector, and system impedance, preventing costly mismatch losses.

RF Cable Types

Right-Angle RF Cable

A right-angle RF cable features a connector with a 90-degree interface, allowing the cable to exit at a perpendicular angle to the mating port. This design is particularly valuable in applications where space is limited, such as inside densely populated equipment racks, portable test setups, or enclosures with restricted clearance behind connectors. By redirecting the cable’s path, right-angle connectors prevent excessive bending of the RF cable near the termination, which helps maintain electrical integrity and prolongs the lifespan of both the cable and the connector.

In many systems, standard straight connectors can strain the mating interface when clearance is minimal. Repeated bending at sharp angles can degrade shielding effectiveness, increase insertion loss, and, in extreme cases, lead to mechanical failure. Using a right-angle RF cable minimizes these risks by managing the bend radius and relieving stress on the connector junction.

Mini-Circuits offers right-angle options across multiple RF cable connector types, including SMA, N-type, and BNC, with frequency coverage up to 26.5 GHz depending on configuration. Our right-angle radio frequency cable assemblies maintain controlled impedance, low VSWR, and excellent shielding performance, even in compact layouts. They are available in flexible, semi-rigid, and low-loss cable constructions to match specific electrical and mechanical requirements.

Whether used in RF test benches, base station installations, or embedded systems, a right-angle RF cable can be a simple yet effective solution to optimize routing, improve durability, and maintain consistent high-frequency performance without compromising accessibility or signal quality.

Low-Loss RF Cable

A low-loss RF cable is specifically engineered to minimize signal attenuation over distance, making it ideal for applications where maintaining signal strength is critical. Attenuation, which is the reduction in signal power as it travels through the cable, is influenced by conductor size, dielectric material, shielding quality, and frequency. Low-loss designs address these factors by using larger diameter conductors for reduced resistance, low-dissipation dielectrics with minimal energy absorption, and high-coverage shielding to prevent leakage.

The benefits of using a low-loss RF cable become most apparent in long cable runs or high-frequency systems where standard cables would introduce unacceptable loss. For example, in base station feeders, point-to-point microwave links, or distributed antenna systems (DAS), every decibel of loss impacts overall system performance. By reducing attenuation, low-loss cables help preserve signal-to-noise ratio, extend transmission distance, and improve link reliability.

In practice, choosing a low-loss RF cable can significantly improve system margins, reduce the need for additional amplification, and ensure that transmitted and received signals retain maximum integrity. They are a high-value choice in demanding commercial, military, and test environments where every fraction of a decibel matters.

BNC to RF Cable

A BNC to RF cable is an assembly that connects a device with a BNC connector to another device using a different RF cable connector type, such as SMA, N-type, or 2.92mm. BNC connectors are widely used in laboratory, broadcast, and instrumentation environments due to their quick-connect bayonet mechanism, which allows for secure connections without threading. This makes them ideal for applications that require frequent connect-and-disconnect cycles.

The BNC to RF cable configuration is particularly valuable in mixed-interface environments. For example, a spectrum analyzer or oscilloscope may have BNC inputs, while the DUT (device under test) or associated RF equipment uses SMA or N-type connectors. Using a well-constructed BNC to radio frequency cable ensures impedance matching (typically 50 ohms for RF systems) and minimal insertion loss between components.

Mini-Circuits manufactures BNC to RF cables with precise impedance control, low VSWR, and excellent shielding to preserve signal integrity from DC to several GHz, depending on the specific connector and cable type. These assemblies are available in flexible, semi-rigid, and low-loss cable options, allowing users to choose the right balance of electrical performance and mechanical flexibility.

Applications for BNC to RF cable assemblies include lab test setups, broadcast video links, and RF prototyping benches. By providing a reliable, pre-terminated connection between BNC and other RF cable connector types, these assemblies eliminate the need for bulky adapters, reduce potential mismatch points, and streamline cable management in high-performance systems.

SMA to SMA RF Cable

An SMA to SMA RF cable is one of the most common interconnects used in RF and microwave systems. The SMA (SubMiniature version A) connector is valued for its compact size, threaded coupling mechanism, and ability to maintain excellent electrical performance up to high frequencies — often 18 GHz for standard designs and up to 50 GHz for precision versions. An SMA-to-SMA radio frequency cable connects two devices with SMA ports, providing a secure, low-loss path for high-frequency signals.

These cables are essential in laboratory environments, production test lines, and field applications where stability, repeatability, and durability are critical. In test setups, an SMA-to-SMA RF cable may link devices such as vector network analyzers, signal generators, and RF modules, where even small variations in performance can impact measurement accuracy.

Mini-Circuits offers SMA-to-SMA RF cables in multiple configurations, including flexible coax for everyday use, semi-rigid options for fixed routing, and armored or phase-stable designs for high-frequency and high-precision testing. All options are available with precise 50-ohm impedance, low VSWR, and excellent shielding effectiveness to maintain signal integrity.

By selecting the right cable construction and length, users can minimize insertion loss, maintain phase stability, and ensure consistent performance over time. Whether for prototyping, system integration, or production testing, an SMA-to-SMA RF cable from Mini-Circuits delivers the mechanical robustness and electrical precision needed for mission-critical RF applications.

RF Cable Sizes

The size of an RF cable is typically defined by its outer diameter (OD) and directly influences its electrical and mechanical performance. Larger diameters generally offer lower attenuation, higher power handling, and improved shielding, but they also reduce flexibility and increase weight. Smaller diameters improve routing flexibility in dense systems but can introduce higher loss, lower power capacity, and reduced durability under repeated bending.

When selecting a radio frequency cable, size must be balanced against application requirements. In test environments, small, flexible cables like Mini-Circuits’ HandFlex® HF047 (0.047” OD) are ideal for tight routing between instruments and DUTs. In contrast, for long transmission runs at high frequencies, low-loss cables like LL405 (0.405” OD) minimize signal degradation over distance.

Factors Influenced by RF Cable Size:

  1. Attenuation: Larger cables reduce conductor resistance and dielectric loss.
  2. Power Handling: Larger conductors dissipate heat more effectively, supporting higher RF power levels.
  3. Flexibility: Smaller cables can bend more easily without damaging the conductor or dielectric.
  4. Connector Compatibility: Cable OD must match the termination’s mechanical specifications for proper strain relief.
  5. Durability: Thicker jackets and larger shields can better withstand environmental stress.

Mini-Circuits’ Approach

We offer RF cables in various sizes to accommodate every performance and mechanical constraint. We recommend smaller-diameter phase-stable cables for precision measurement to avoid flexure-induced phase shifts. For outdoor or base station use, larger low-loss cables provide the best balance of low attenuation and high durability.

Selecting the correct RF cable size is not simply about physical fit but ensuring the cable’s electrical properties match your system’s requirements. Oversizing can waste space and budget, while undersizing can compromise signal quality and shorten the assembly’s service life. The optimal choice depends on frequency, run length, required flexibility, and the RF cable connector types used in the system.

Summary: How to Choose the Best RF Cable for My Application?

Selecting the best RF cable for your application requires a structured approach that balances electrical performance, mechanical constraints, and environmental durability. Choosing incorrectly can lead to degraded signal integrity, system downtime, or costly rework, while the right choice ensures optimal performance and long-term reliability.

At Mini-Circuits, we recommend following these steps when deciding which radio frequency cable and RF cable connector types to use:

1. Define Your Frequency Range

The cable must perform effectively at your highest operating frequency. Attenuation rises with frequency, so a cable suitable at 1 GHz may be unacceptable at 40 GHz. Review attenuation charts and loss data to ensure your selected RF cable meets your loss budget.

2. Establish Your Loss Budget

Determine how much signal loss is acceptable between the source and load. Compare candidates using an RF cable attenuation calculator or loss chart. If loss exceeds your limit, consider a low-loss or larger-diameter option.

3. Select Appropriate RF Cable Connector Types

Connector choice affects both electrical and mechanical performance. SMA, N-type, 2.92mm, and BNC each have different frequency limits, durability, and coupling methods. Matching connectors to your system interfaces reduces the need for adapters and minimizes potential mismatch points.

4. Consider Environmental Conditions

Outdoor installations may require weatherproof jackets, UV resistance, or armored designs. High-vibration environments may call for ruggedized or semi-rigid cables. In temperature-sensitive systems, use materials rated for your thermal range.

5. Factor in Mechanical Requirements

Minimum bend radius, flexibility, and weight all matter. Tight equipment racks may benefit from right-angle connectors, while portable setups may require ultra-flexible cables like HandFlex®.

6. Decide Between Standard and Custom RF Cables

If your needs are highly specific — such as phase-matched assemblies for phased arrays or unique connector combinations — a custom RF cable may be the most effective solution.

Example Decision Path:

  • Application: 28 GHz 5G base station feeder line, 5 meters
  • Constraints: Low loss, outdoor use, high durability
  • Choice: LL405 Low-Loss RF Cable with N-type connectors, weatherproof jacket, attenuation < 2 dB total

Mini-Circuits Makes It Easy
We provide detailed specifications, attenuation charts, and engineering support to ensure you make the right selection. Our broad portfolio — from flexible lab jumpers to armored, low-loss cables for field deployment — allows us to match the right radio frequency cable to any application.

The best RF cable meets your electrical requirements, fits your mechanical constraints, survives your environmental conditions, and integrates seamlessly into your system architecture. With careful evaluation and the right partner, your cable becomes a reliable, high-performance signal path rather than a limiting factor in your design.

Power your signal with Mini-Circuits. Shop precision RF cables built for unmatched performance. Order Now »