by Rinchen Athup | Sep 5, 2025 | Cables, Engineering Resources, Product Updates
DC TO 18 GHz Great Quality. Better Value. >15% Price Reduction on Test Cables! Has the cost of your test cables increased? Not if you’re using ours! Mini-Circuits has reduced list pricing of its popular CBL-series of 18 GHz test cables to give you the same product...
by Rinchen Athup | May 30, 2025 | Cables, Engineering Resources, Product Updates
DC TO 26.5 GHz Phase-Stable Flex Cables For Precision Test Applications Mini-Circuits’ new CBN-series of phase-stable flexible cables supports a wide range of precision test applications from DC to 26.5 GHz. CBN-series models provide exceptional phase and amplitude...
by jacquelineh96 | Apr 1, 2025 | Adapters, Cables, Engineering Resources, Measurement Methods & Techniques, Test Solutions
The Best Way to Connect The performance of every RF system depends on the quality and application of each component. In industry, much of the focus is on complex, expensive RF equipment. At the same time, it is also prudent to give equal attention to the quality and...
by Rinchen Athup | Mar 7, 2025 | Adapters, Cables, Engineering Resources
1.0 Proper Handling of 1.0 mm Interconnections 1.0 mm connectors require care, precision and that proper methodology be utilized when making interconnections between cables, adapters and equipment. These connectors are high-precision mechanical devices that are...
by Rinchen Athup | Feb 28, 2025 | Cables, Engineering Resources, Product Updates
DC TO 110 GHz 1.0mm M-F Armored Cables Double-Shielded with Low Insertion Loss & VSWR Mini-Circuits’ line of 1.0 mm-terminated coaxial cables includes a half dozen lengths and connector mating adaptations to meet all possible interface requirements. Ultra-wide...
by jacquelineh96 | Aug 27, 2024 | Cables
Phase-matched cables ensure signal propagation from phased array antennas is straight. Phase-matched cable assemblies are ubiquitous, and modern-day phase matching requirements serve to drive their growing popularity. As electrical length matching requirements have...
You must be logged in to post a comment.