Engineering Resources
Filter By Category:

1.35mm DC to 90 GHz Adapters
Mini-Circuits’ 1.35mm to 1.35mm RF/mmWave adapter series offers three mating adaptations to meet all possible interface configurations. Ultra-wideband, 90 GHz capability allows these units to be integrated into a variety of system types

Selecting VCOs for Clock Timing Circuits – A System Perspective
Clock Timing, Phase Noise and Bit Error Rate (BER)
Timing is critical in digital systems, especially in electronic systems that feature high-speed data converters and high-resolution sampling. A clock source is the “timekeeper” and the system

Wideband MMIC Variable Gain Amplifier
The PVGA-273+ low noise, variable gain MMIC amplifier features an NF of 2.6 dB, 13.9 dB gain, +15 dBm P1dB, and +29 dBm OIP3. This VGA affords a gain control range of 30 dB with a control voltage of -0.7 to 2.0V.

Fast-Switching GaAs Switches Are a High-Performance, Low-Cost Alternative to SOI
While many MMIC switch designs have gravitated toward Silicon-on-Insulator (SOI) technology due to its ability to achieve fast switching, high power handling and wide bandwidths for high-frequency operating bands, many commercially available options on the market come at high cost.

Measurement of Amplifier Phase Noise (APM)
In our efforts to characterize the additive phase noise performance of our MMIC amplifier product line, Mini-Circuits has devoted considerable attention to the measurement methods and techniques we use to capture accurate data for these notoriously sensitive parameters. This article provides a deep dive into our measurement setup and process for characterizing additive phase modulation noise (APM) and additive amplitude modulation noise (AAM) in our labs.

UHF to mmWave Cavity Filter Solutions
Cavity filters achieve much higher Q, steeper rejection skirts, and higher power handling than other filter technologies, such as ceramic resonator filters, and are utilized where low passband insertion loss and high rejection of neighboring channels/spurious emissions are critical.

Frequency Modulation Fundamentals
The development of crystal-clear FM communications was an innovation of genius and toil. Utilized today in applications such as radar, seismology, telemetry and two-way radios, FM remains a ubiquitous real world technology because of its superior signal to noise ratio compared to other modulation schemes. Read on to learn about the history, theory and illustrative use cases including FM radio and the radar altimeter.

44 GHz Programmable Signal Generator
The Mini-Circuits’ SSG-44G-RC is a 0.1 to 44 GHz signal source with an RF output range of -40 to +17 dBm with fine resolution. This model supports CW and pulsed (≥ 0.5 μs) outputs while sweeping and hopping between power levels and frequencies.

50W SSPA with Built-In Signal Source & Control
The RFS-2G42G5050X+ takes Mini-Circuits’ robust line of solid state, connectorized, high-power amplifiers for RF energy to a new level by integrating the versatility of a signal generator with a 50W amplifier. The ruggedness of the RFS-2G42G5050X+ is enhanced by the built-in monitor and control circuitry which protects the module from excess temperature, current, supply voltage, forward and reverse power.

The Basics of Orthogonal Frequency-Division Multiplexing (OFDM)
While traditional Frequency Division Multiplexing has been around for over 100 years, OFDM was first introduced by Robert W. Chang of Bell Laboratories in 1966.1,2,3,4 In OFDM, the stream of information is split between many closely-spaced, narrowband subcarriers instead of being relegated to a single wideband channel frequency.

Mesh Network Simulators Up To 16 Ports
Mini-Circuits has expanded our range of test systems for characterizing wireless mesh network devices, now with standard configurations up to 16-ports built to order with fast turnaround. All external ports of the mesh are interconnected to simulate an over-the-air wireless mesh configuration.

High Pass Filters – Compact, Cost-Effective and Extending to 60 GHz
When designing mmWave frequency systems that span Q-band and half of V-band, engineers are often faced with difficult tradeoffs when it comes to filter selection. Mini-Circuits has broken through with our HFCQ (1008), HFCN (1206) and HFCV (1210) series high pass filters. These latest LTCC filters from Mini-Circuits exhibit passbands that cover Q-band and the lower half of V-band while offering a combination of insertion loss, return loss, rejection, size, cost, repeatability, ruggedness and reliability that has only now become available.