Q. Please describe the spectrum at the output of a limiter.

A. Since a limiter acts in a saturated mode, its output contains many harmonics of the applied input signal. The harmonic content is a function of the bias current and applied power level.

This image has an empty alt attribute; its file name is lim102_01.png
Figure 1

Q. Will a DC component in the input signal influence limiting action?

A. No. The input port is at DC ground.

Q. How is the output level of the limiter affected by control current?

A. The output level will increase for increased values of control current, as shown.

This image has an empty alt attribute; its file name is lim102_02.png
Figure 2

Q. What is the effect of using a 50Ω limiter in a 75Ω system?

A. This approach is generally recommended because there will be a small change in limiting action. The efficiency of limiting would not be compromised.

Q. What happens in a limiter if signals other than a sine wave are applied?

A. As long as the input level is of sufficient amplitude the diodes will saturate and limiting will occur. The limiting efficiency of output/input will most likely be affected and would be a function of the input wave shape.

This image has an empty alt attribute; its file name is lim102_03.png
Figure 3

Q. Is it possible to obtain Mini-Circuits’ limiters in a surface-mount package?

A. Yes. You may select anyone of our surface-mount packages in the handbook. Please refer to the mixer, Section 1, for various packages available.

Q. What is meant by the dynamic range of a limiter?

A. The dynamic range indicates the variation of RF input power over which a limiter will maintain a relatively constant output level.

Browse all RF limiters

%d bloggers like this: