Relationships of VCO Performance Parameters

A. Parameters Affecting VCO Frequency Range the Following Parameters Affect the VCO Frequency Range.
A.1. TUNING VOLTAGE
• An increase in tuning voltage range widens frequency range.
A.2. TUNING SENSITIVITY
• Lower sensitivity means a narrower frequency range for a given range of tuning voltage.
A.3. PUSHING
• Increased pushing causes decreased effective frequency range.
A.4. PULLING
• Increased pulling causes decreased effective frequency range.
A.5. TEMPERATURE
• An increase in the range of the ambient operating temperature causes a decrease in the VCO’s frequency range and vice-versa.
B. Parameters Affecting VCO Power Output. The following parameters affect the VCO Power Output:
B.1. SUPPLY CURRENT
• Increasing supply current typically increases power output B.2.
PULLING
- To improve pulling, output power should be reduced by connecting an attenuation circuit at the VCO output.
- Improved pulling can also be achieved by connecting a buffer amplifier at the VCO output port. However, this buffer amplifier requires a higher supply current.
B.3. TEMPERATURE
• From an ambient temp of +25°C: a temp increase to +85°C results in an output power decrease of 0.5 dB to 1.0 dB typically.
• From an ambient temp of +25°C: a temp decrease to -55°C results in an output power increase of 0.5 dB to 1.0 dB typically.
C.The Following Parameters Affect the VCO Power Output Flatness:
C.1. FREQUENCY BANDWIDTH
• As the VCO frequency range is increased, the difficulty to achieve a flat output power is increased.
C.2. TUNING VOLTAGE
• As the tuning voltage range is reduced and narrowed, a flatter output power can be achieved.
C.3. TUNING SENSITIVITY
• It is more difficult to achieve flat output power for high tuning sensitivity than for low tuning sensitivity.
C.4. HARMONICS
• Adding an output filter to suppress harmonics may in some cases degrade power output flatness.
D. The Following Parameters Affect the VCO Tuning Sensitivity:
D.1. FREQUENCY RANGE
• For a given tuning voltage range, increasing the frequency range requires an increase in the tuning sensitivity, and vice-versa.
D.2. TUNING VOLTAGE
• For a given frequency range, increasing the tuning voltage range decreases the tuning sensitivity, and vice-versa.
E. The Following Parameters Affect the VCO Supply Current:
E.1. POWER OUTPUT
• Increasing power output requires higher supply current.
E.2. PULLING
• Same as B.2.
E.3. TEMPERATURE
• From an ambient temp of +25°C: a temp increase to +85°C typically results in a supply current increase of approximately 10%.
• From an ambient temp of +25°C: a temp decrease to -55°C typically results in a supply current decrease of approximately 10%.
F. The Following Parameters Affect the VCO Pushing:
F.1. FREQUENCY
• As the VCO frequency increases, difficulty in achieving good pushing is increased.
F.2. POWER SUPPLY
• Good pushing is easier to achieve in designs with high current.
G. The Following Parameters Affect the VCO Pulling:
G.1. FREQUENCY
• As the VCO frequency increases, difficulty in achieving good pulling is increased.
• See B.2.
G.2. SUPPLY CURRENT
• It is difficult to achieve good pulling when there is a limit on supply current consumption, due to the fact that (connecting a buffer amplifier at the VCO output port) improving pulling increases current consumption.
H. The Following Parameters Affect the VCO Modulation Bandwidth:
H.1. FREQUENCY
• Higher modulation bandwidth can easily be achieved at higher frequency.
I. The Following Parameters Affect VCO Harmonics Suppression:
I.1. FREQUENCY BANDWIDTH
• It is easier to achieve good harmonics suppression when frequency range is narrow.
I.2. TEMPERATURE
• With ambient temperature increase, the harmonic level gets lower. With ambient temperature decrease, the harmonic level gets higher.
J. The Following Parameters Affect VCO Phase Noise:
J.1. FREQUENCY
• As carrier frequency increases, it’s more difficult to achieve good phase noise.
J.2. FREQUENCY RANGE
• It’s easy to achieve good phase noise when frequency range is narrow.
J.3. TUNING SENSITIVITY
• Increasing the tuning sensitivity degrades phase noise and vice-versa.
J.4. SUPPLY CURRENT
• It is typically easy to achieve good phase noise at higher offset frequencies (> 1 kHz) in designs with a high supply current.
J.5. TUNING VOLTAGE
• For a given frequency range it is typically easy to achieve good phase noise in designs with a wide tuning voltage range.
J.6. TEMPERATURE
• Phase noise varies typically by 3 dB in the -55°C to +85°C range.
J.7. PUSHING
• High pushing can cause phase noise degradation due to increased sensitivity to the power supply noise.

Browse all voltage controlled oscillators (VCO’s)