Introduction

Monolithic microwave amplifiers are widely used in the industry for signal amplification. The majority of these amplifiers are specified to operate with fixed current. In the real world of low voltage supplies, fixed current is difficult to realize. Normally, a constant current source is approximated by a voltage source, RF choke and a resistor. In addition, DC blocking capacitors need to be added at the input and output of such amplifiers. All these external elements consume real estate on the user’s PC board, and increase the component count, cost and complexity of the design. To address these issues, Mini-Circuits is introducing a series of fully integrated amplifiers, which operate with a fixed voltage source. Besides being easy to use, these amplifiers have very low profile and extremely high isolation. The later feature helps an amplifier to be used as an active isolator. This article presents the performance and describes the advantages of this new series of amplifiers.

Biasing of Monolithic Microwave Amplifiers

Figure 1: Biasing circuit of most monolithic microwave amplifiers.

Figure 1 shows the biasing circuit of most of the commercially available monolithic amplifiers. These amplifiers are designed for fixed current operation, and the DC bias current has to be applied at the RF output terminal. Therefore, it is important to ensure that the biasing circuit does not load the RF output (by proper selection of RFC and Rbias), and that the DC current does not go to the RF load (C-block prevents it). The combined reactance of RFC and Rbias should be greater than 500Ω to prevent reduction of gain and power output. The RFC should also have its resonant frequency higher than the intended frequency of operation. In addition, a DC blocking capacitor is needed at the input to prevent DC current flow back into the signal source. A minimum of 2V drop across Rbias is required for proper operation.

The new MNA series of monolithic microwave amplifiers that Mini-Circuits is introducing are well matched to 50Ω; they are wide band and much simpler to use. This makes them very user friendly. Unlike current operated amplifiers, the new series has separate terminals for the RF output and DC supply. In addition, these new amplifiers are designed to operate with a fixed voltage source rather than a fixed current source. Figure 2a shows the primary biasing circuit of the new amplifier series. Note that the only external component is a bypass capacitor for the DC supply, which provides an RF ground at the amplifier DC terminal. The capacitor, as well as the short between Pins 7 and 8 should be located as close as possible to the MNA amplifier. To ensure unconditional stability (a concern only for model MNA-4), the alternative biasing circuit in Figure 2b is recommended. This alternative circuit has the advantage, for all models, of preventing possible resonance between internal and external biasing components. Chip components of 0402 or 0603 size are recommended, and should be located within 100 ml (2.5mm) of the amplifier package. A test board that includes the Figure 2b biasing circuit is available; the Mini-Circuits “Specification Sheet” shows the recommended PC board layout. The effect of biasing circuit on electrical performance is described later in this article.

Figure 2: Biasing circuits of new monolithic amplifier.

The physical dimensions of these amplifiers are 3 mm x 3 mm x 0.89 mm, or 0.118” x 0.118” x 0.035”. This small size saves board space. The MNA amplifiers have a bottom paddle, which is soldered directly to the PC board of the customer’s circuit to provide lowest thermal resistance. Figure 3 illustrates the new MNA amplifier.

Figure 3: Photograph of MNA amplifier.

Electrical Performance

Table 1 shows the typical specifications of these amplifiers. One significant feature is that they can be operated over a wide voltage range, 2.8 to 5V. This makes them useable for battery powered applications.

Table 1: Specifications (typical) of MNA series amplifiers supply voltage: 2.8 to 5V.

The MNA series offers a choice of gains and power output to aid the circuit designer. Detailed specifications of these amplifiers can be found on individual model datasheets.

MNA-7 is a high frequency amplifier operating over 1.5 to 5.9 GHz. This wide frequency range covers applications from PCS at the low end to satellite communication at the high end, and a variety of other applications in between such as defense, ISM etc. MNA-7 has all the features of its low frequency counterparts.

Figure 4 shows the gain of the MNA-4 amplifier, for example, at two different voltages: 2.8 and 5V. Note that the gain change is only 2 dB for such a drastic change of supply voltage. Figure 5 shows the reverse isolation of the same amplifier; it is in the range of 30 to 45 dB across the band. This is equivalent to an active directivity of 15 to 30 dB, which enables these amplifiers to be used as low cost active isolators. Some applications for high isolation amplifiers are reducing load pull of voltage controlled oscillators, providing a broadband interface at the input and output of filters that are reflective in their stop-bands, and any situation where mismatch could degrade system performance. Figures 6 and 7 show the VSWR at input and output. The amplifiers are well matched over 700 to 2500 MHz. This makes them extremely simple to use. Figure 8 shows the 1 dB output power compression of the MNA-4 amplifier.

Note that the trade-off of output power with choice of supply voltage is well defined; the difference is about 5 dB at low frequency and 2.5 dB at the high frequency.

Figure 4
Figure 5
Figure 6
Figure 7
Figure 8

Effect of Biasing Circuit on Electrical Performance

Figures 9a, b, c through 14a, b, c show gain, input return loss, and output return loss of models MNA-2 through MNA-7 vs. frequency out to 6 GHz. Each graph plots the performance of two samples using the primary bias circuit (Figure 2a), as well as the same two samples using the alternative biasing circuit (Figure 2b).

MNA-2 and MNA-6 have slightly lower gain up to 3 GHz and up to 2 GHz respectively, with the alternative biasing circuit. MNA-3, MNA-4, and MNA-5 show decreased gain with the alternative biasing circuit only below 1 GHz, and the effect is to smooth the response by eliminating a tendency of the gain to peak. MNA-7 does not show a significant difference in the gain, but the alternative biasing circuit provides smoother return loss response at high frequencies.

Figure 9
Figure 10
Figure 11
Figure 12
Figure 13
Figure 14

Reliability

The thermal resistance of these amplifiers, from junction to case, is 780 ℃ / W. For the 17 dBm output MNA amplifiers this results in a junction temperature rise of 35°C above the case. At 85°C case temperature the junction temperature is thus 120°C, which makes the amplifier extremely reliable. When soldered on a PCB the amplifier case temperature typically rises 100℃ above ambient, making the junction temperature 130°C. From Figure 15 the MTTF is around 2000 years at this temperature. For the lower power MNA models, junction temperature is lower so there is no need for concern about MTTF, as it is extremely high.

Figure 15: MTTF vs. junction temperature.

Conclusion

Mini-Circuits has introduced a series of new amplifiers to cover 0.5 to 5.9 GHz. These amplifiers have a separate terminal for DC, and require no external matching, biasing or DC blocking elements. They operate with fixed DC voltage and have very high reverse isolation. These tiny amplifiers will save circuit space and are simpler to use.

Browse all RF amplifiers

%d bloggers like this: