Recent disruptions in the supply base for ceramic resonators have sent waves of end-of-life notifications through the RF component market. Customers utilizing ceramic-resonator-based filters and other parts are left with the problem of finding alternative suppliers or redesign their systems. Ceramic resonator filters’ sharp selectivity and deep rejection floor for narrow passbands allows frequency responses precisely tuned to customers’ unique requirements in a small, surface-mount form factor. But because passbands are often tailored to meet specific customer requirements of a given application, they tend to be purpose built for a given application, making second-sourcing an especially difficult challenge.

While many customers are working around the impact of industry consolidation and factory closures, Mini-Circuits’ supply chain for ceramic resonators remains unaffected by these changes elsewhere in the market, and our customers will see no delays or disruptions in orders for ceramic resonator filters. We offer a wide selection of models from stock and have decades of experience designing custom filters for special requirements. Our manufacturing organization has the capacity to support additional customer demand and accommodate customers seeking a partner to replace filters facing obsolescence in their designs. Our knowledgeable applications engineers, regional sales teams and authorized reps are ready and able to assist with part selection, quotes, lead times and other issues that may impact your design and production.

For over 35 years, Mini-Circuits has been the solid source for your filtering needs with one of the industry’s most extensive in-house design and manufacturing capabilities. We offer nine different filter technologies, including ceramic resonator, cavity, lumped L-C, LTCC, MMIC reflectionless, stripline/microstrip, suspended substrate, thin film on alumina and waveguide. We’re proud to offer over 1500 unique filter models from stock plus affordable custom designs with fast turnaround and the assurance of support through the life of your system.

Pattern made of repeating ceramic resonator filters at different angles with a button reading "Explore Ceramic Resonator Filters"

Related Content:

Understanding Ceramic Coaxial Resonator Filters

Ceramic coaxial resonators boast two parameters: quality factor (Q) and dielectric constant (ϵr) that are so impressively high as to explain why these resonators have become standard building blocks for bandpass and bandstop filters for over four decades.

Read More >

Filtering Solutions for 5G C-Band Interference with Radar Altimeter Receivers

Recent debate about potential interference between 5G network equipment operating in C-band frequencies and radar altimeter (RA) receivers onboard commercial aircraft has highlighted the need for high-Q filtering solutions in crowded spectral environments. Mini-Circuits has developed ceramic resonator and cavity filters specially designed to eliminate interference by 5G C-Band emissions when incorporated either within or in line with the RA assembly. 

Read More >

High-Q Ceramic Resonator Filters for GNSS Applications

Filters for GNSS systems must exhibit high rejection with high selectivity . Narrow bandwidths are ideal for L-band applications where spectrum allocations are crowded, and low insertion loss is important for processing the relatively weak signals transmitted from satellites to receivers on Earth. Ceramic resonator technology offers the ideal combination of performance, size and cost to meet the requirements of these demanding applications.

Read More >