Introduction

Mini-Circuits manufactures a wide range of 4-pin MMIC surface-mount and drop-in amplifiers. A family of test boards for evaluating these devices has been designed to make them easy to use by customers.

On the board, all components external to the amplifier, such as bias resistors, DC blocking and bypass capacitors and RF chokes, together with the amplifier have been placed and soldered onto the test board. In this board, measured performance of the device under test is affected by these external components. Tables 2.1 – 2.3 show the loss of test board. Add the values given in 3 (table 2.1, column 3) for respective models to the measured gain to get actual amplifier gain.

General Schematics

MMIC amplifiers have different device voltages and operating currents. This test board has been configured to use a fixed supply voltage, 12V, irrespective of the amplifier. DC current flowing through the amplifier is set by suitable selection of bias resistors.

Table 1: Test board components.
Note: Location of index depends on model.

Procedure for Using Test Board

Follow these steps to use the test board:

  1. Calibrate the network analyzer.
  2. First, connect the RF output port of the test board to the network analyzer.
  3. Then, apply +12V DC.
  4. Finally, connect the RF input port of the test board to the network analyzer and apply RF input. Gain is now displayed on the network analyzer.

Test Board Loss

Table 2.1: Insertion loss of test board for ERA, MAR,RAM, and GALI amplifiers.
Table 2.2: Insertion loss of test board for LEE amplifiers.
Table 2.3: Insertion loss of test board for MAV amplifiers.

Amplifier and Test Board Cross Reference

Browse all MMIC amplifiers

%d bloggers like this: