The PGA-103+ is a monolithic amplifier for the 50-4000 MHz range with excellent noise figure and a high dynamic range (1 dB compression point: 22.5 dBm and ultra-high OIP3, 44 dBm typ. @ 2GHz). Due to the intrinsic nature of the GaAs PHEMT, it is not unconditionally stable (stability factor k>1 and stability measure B>0) as k.

In order to improve stability additional components need to be added at input, see Figure 2 and associated component values in Table 1.


The stability parameters of the amplifier with the stabilizing network are shown in Figure 3. Note: k>1 and B>0 over entire range.
The performance of the stabilized amplifier:
Performace with and without stabilization is shown in Figures 3 – 11:









Conclusion
- Use of the stabilization circuitry has minor impact on all parameters.
- The use of the stabilization circuitry guarantees amplifier’s unconditional stability.
Browse all MMIC amplifiers