Engineering Resources

Filter By Category:

50W µCeramIQ® Couplers in Tiny SMT Package

50W µCeramIQ® Couplers in Tiny SMT Package

Mini-Circuits’ µCeramIQ® high-power coupler series delivers an uncommon combination of 50W power handling and a tiny, surface-mountable LTCC monolith. Designed for systems where SWAP requirements are critical, these couplers provide stable, repeatable performance while supporting modern, high-volume assembly processes.
>70 dB Rejection µCeramIQ High Pass Filters

>70 dB Rejection µCeramIQ High Pass Filters

Our innovative high-rejection µCeramIQ filter line continues to redefine what’s possible in a variety of applications, giving designers outstanding filter rejection and selectivity at a fraction of the size and cost of competing filter technologies. We’ve expanded our selection to accommodate your needs by adding several new models to the HFHKI-family of high-pass filters..
Product Highlight: ZVA-24443HP+ Ka-Band Amplifier (24 – 43.5 GHz) with 47 dB Gain and 2.2 dB Noise

Product Highlight: ZVA-24443HP+ Ka-Band Amplifier (24 – 43.5 GHz) with 47 dB Gain and 2.2 dB Noise

In this product highlight, Mini-Circuits Product Line Engineering Manager, Dan Ford shares an overview of the ZVA-24443HP+ Ka-Band Amplifier, supporting applications from 24 to 43.5 GHz with high gain, low noise figure, and +29 dBm output power at saturation. This model is an ideal solution for applications including wideband test and instrumentation, Ka-Band satellite communications (Satcom), broadband / 5G telecommunications networks and more. About Mini-Circuits: Mini-Circuits is the world’s preferred supplier of RF and microwave components and systems. With 14 design, manufacturing and sales locations in nine countries, as well as hundreds of sales channel partners worldwide, Mini-Circuits offers 27 product lines comprising over 10,000 active models. Over 20,000 customers choose Mini-Circuits for the demanding quality standards, world-class customer support, on-time delivery and value pricing that have earned the industry’s trust for over 50 years. More from Mini-Circuits: Visit Mini-Circuits’ website: https://www.minicircuits.com/ Like Mini-Circuits on Facebook: https://www.facebook.com/MiniCircuits Follow with Mini-Circuits on LinkedIn: https://www.linkedin.com/company/mini-circuits Follow Mini-Circuits on X: https://twitter.com/MiniCircuits Follow Mini-Circuits on Instagram: https://www.instagram.com/minicircuits/
1.5×1.5mm MMIC Slope Equalizers

1.5×1.5mm MMIC Slope Equalizers

Mini-Circuits has expanded its EQY-series GaAs MMIC gain equalizers with new models operating from DC to 12 GHz in ultra-compact 1.5 x 1.5 mm QFN-style package. Available in a wide selection of linear positive slope values with excellent return loss performance, these devices provide ideal solutions for compensating negative gain roll-off in wideband systems
SATCOM Shifts Reference Frequency from 10 to 100 MHz – A System Perspective

SATCOM Shifts Reference Frequency from 10 to 100 MHz – A System Perspective

Over the last decade, the satellite communications (SATCOM) industry has been evolving to support both wider channel bandwidths (BWs) and higher order modulations such as higher order quadrature amplitude modulation (QAM). The increasing constellation density of higher order QAM raises its sensitivity to phase jitter, which will also degrade the system BER if lower system phase noise is not first achieved. To achieve higher data throughput by correspondingly reducing system phase noise, many in the SATCOM industry have been moving the reference frequency of their distribution clocks and subsystem timing architectures away from the long-standing 10 MHz reference and toward higher-frequency references such as 100 MHz. Mini-Circuits supports this migration path with our line of Bias-Tee/Diplexers that are ideal for SATCOM installations.
Connectorized Evaluation Modules for MMIC Devices

Connectorized Evaluation Modules for MMIC Devices

At Mini-Circuits, we strive to provide the best engineering resources to help you evaluate our products for your specific applications. We’ve compiled this convenient cross-reference to help you identify connectorized modules corresponding to surface-mount MMICs of interest at a glance.
Product Highlight: ZVE 18GB+ Wideband RF Low Noise Amplifier (LNA) with High Linear Output Power

Product Highlight: ZVE 18GB+ Wideband RF Low Noise Amplifier (LNA) with High Linear Output Power

Dan Ford, Mini-Circuits' Engineering Manager, explains the unique features of the ZVE-18GB+ wideband low noise amplifier. Operating from 0.1 to 18 GHz, this model provides high linear output power and low noise, improving overall system signal-to-noise ratio.
Part 4: 2025 Low Level RF (LLRF) Workshop – Amplifier Additive Phase Noise Measurement Tutorial

Part 4: 2025 Low Level RF (LLRF) Workshop – Amplifier Additive Phase Noise Measurement Tutorial

Mini-Circuits R&D Fellow, Joe Merenda delivers an in-depth tutorial on the fundamentals of RF amplifier additive phase noise theory, measurement setup, and differences between small and large signal APN behavior, including practical examples of additive phase noise in cascade designs.
RF Signal Quality Measurements: Third-Order Intercept Point (IP3) and Power at 1 dB Compression (P1dB)

RF Signal Quality Measurements: Third-Order Intercept Point (IP3) and Power at 1 dB Compression (P1dB)

RF signal quality is a key concern when building an RF system. Most RF systems and are designed and built to operate in the linear range. The linear range is the region of operation where the output power is some constant multiple of the input power. When the input is driven past the linear region, non-linear behaviors begin to develop, mainly the generation of harmonics and intermodulation products at the output of the device.
100+ Ceramic Resonator Filters for High Selectivity Applications

100+ Ceramic Resonator Filters for High Selectivity Applications

Mini-Circuits’ ceramic coaxial resonator filters offer low insertion loss in very small form factors, using ceramic material with high dielectric constant and superior Q factor. Bandpass and bandstop filters, diplexer and multiplexer designs can be constructed using this technology. Low insertion loss combined with excellent power handling makes these filters well suited for transmitter and receiver signal chains.
Lexicon of Balun and Transformer Configurations

Lexicon of Balun and Transformer Configurations

RF baluns and transformers may be some of the most challenging components to select for a given system design. For starters, baluns and transformers are used for a wide variety of functions which partly determine the appropriate configuration for a given application.
Configure your Ideal Test System Online – Fast Quote & Delivery

Configure your Ideal Test System Online – Fast Quote & Delivery

Mini-Circuits’ modular switch systems offer flexibility, customizable functionality and fast turnaround for automated test setups. Choose one of our standard benchtop or rack-mount chassis structures and configure your system with our industry-leading range of rugged and high-performance mechanical switches, programmable attenuators and more.